Thanks waltr fro helping here!
Dragon OSD+ uses 115200 8N1. This is a TTL compatible voltage level, but running standard UART serial protocol, at 8-bits, No parity, 1 stop bit - hence 8N1. (that’s what I’ve set to modules and everywhere
)
in X-CTU test doesn’t go through, get all BAD packets. Somehow I can’t connect to another module or I don’t know what I am doing. It is so difficult to understand thins in this new era 
I can’t tell more about PC Commander software, I just choose COM port and that’s it.
I am using this setup:
WRL-09132 XBee Explorer Regulated
WRL-09819 XBee Explorer Dongle
WRL-08742 XBee Pro 60mW Wire Antenna
WRL-08710 XBee Pro 60mW U.FL Connection
From Explorer Regulated i have 3 wires (tx,rx,gnd) connected to DOSD UART serial.
I’ve checked those 2 modems are exact the same. firmwares and models.
Can you please give some ideas on hook them up? Thanks
Any other faster way to test them?
This what i am doing 
http://www.vimeo.com/20024265 (there are more videos)
Thanks in advance!
Virgis
waltr:
using XBEE PRO 802.15.4 10CD version
Good, with this we know exactly which XBee you have.
Take it a step at a time.
Does the XBee respond to a Test/Query from X-CTU?
What Baud rate have you set? Are the other serial parameters, #bits, Stop bit, correct for what you are interface to?
PC Commander software (using COM port)
Is this a terminal program? Does the XBee respond to the "+++" command string with an "OK"?
I am setting them up to work Dragon OSD+
I don't know what this is but assume it has an asynchronous serial port at TTL levels. Is this correct?
Does the Baud rate of the Dragon OSD+ match the XBee?
Does the Dragon OSD+ work when connected to the PC with the XBees?
Have you searched this forum and read the many posts and links? There is lots of info on getting XBees working here.