I’ve recently bought two Xbee Pro 900Mhz and the breakout board for it. I’m having some trouble getting it to communicate with the computer. I hooked it up to FTDI. But when I go to hyperterminal and type +++, I get no response. When I try X-CTU, it tells me unable to communicate with modem. I’ve tried both breakout boards and both Xbees. I’ve tried two different FTDI. I’m out of ideas. Anybody know what the problem might be, or something I can try? Thanks.
Edit: Also, the breakout board power led comes on, so I know the thing is getting power.
Yep. I tried Test/Query with the proper com port selected, baud rate and others at default and every possible variation. I get unable to communicate with modem.
recently, I had an XBee 900MHz board with these symptoms. Digi support and I worked with my official Digi development kit's XBee to RS232 board and tried to revive it. Support guy did the death certificate for that one.
EDIT: re the next post down… my comment, above, is N/A because above, I wasn’t using the SFE board. It’s been discussed many times that the SFE board’s diode in the serial data path isn’t correct for proper logic levels.
I found a solution to the problem. It was previously answered on the forum:
Excalbian:
After opening a support ticket with Digi (they directed me to update the firmware which also didn’t work), someone else (on an R/C UAV forum) suggested that a solution he’s found is to short out the diode in front of Din. Sure enough, as soon as that was done, not only could I read and write the module from XCTU but it worked with the other module as a transceiver.
So I did just that, shorted out the diode in front of DIN on the Sparkfun Explorer Regulated (for some reason the placement of the diode was either improper or not necessary-most likely placed in the wrong direction).