Hi,
this is a crosspost:
I have a XBEE 3 Micro (XB3-24Z8CM Rev C) soldered on a custom PCB. The Xbee is connected to an Teensy 3.2.
I can’t connect to it via serial connection. I am using ‘+++’ to get into AT mode, but get no answer.
My serial seetings are 8n1 at 9600 Bauds/s.
I made the following connections:
GND to Teensy GND
VCC to Teensy 3v3
DOUT to Teensy RX
DIN to Teensy TX
Using an oscilloscope, i get the following signals on the pins:
1.GND) 0V
2.Vcc) +3v3
3.DOUT) 0V
4.DIN) my serial signal (‘+++’)
- +3v3
6.RESET) +3v3
7->19) 0V
20.RSVD) +3v3
22->34) 0V
I’m especially surprised that I’m getting 0V on the ON-pin.
What am I doing wrong?