I have an uno, XBee, and Xbee shield and want to the Xbee to send True or False to my computer (a webpage–isn’t there an open webpage that I can stream data to somewhere?) based on if the LED is on or off (with LEDBlink program modified).
Since the Xbee comes with default configuration settings I should be able to set the correct COM, and baud and my computer connect/recognize the Xbee but when I plug my arduino in with the Xbee shield and use my IP scanner I don’t see its IP address show up anywhere. Where is my understanding wrong?
I tried but my Xbee isn’t showing up–I should be able to just connect with the default configuration settings but the the test query doesn’t work. (see pic)
I don’t have the explorer for configuration. I just have it plugge into my arduino but was under the impression I could just use its default configuration settings and connect to it.
Only the UNO(COM3) comes up in my device manager so I reinstalled the drivers (the one ones for windows7 at the bottom of the page http://www.digi.com/support/productdetl … s=358&tp=1) and put them in the drivers folder where my UNO drivers are located but am still only seeing UNO show up in my LPT+COM