Hello,
I have a pair XBee modules and BASIC Stamps that I need to conect for
a project I’m working on, but I must first address the logic level
issue; that is, the BASIC Stamp’s logic level of five volts is, naturally,
incompatible with the XBee’s three.
The SelmaWare AppBee-Mod uses the 74LVC244A “logic buffer” for logic level
conversion, but I can’t find a detailed schematic; just pictures. The
SparkFun logic level converter (http://www.sparkfun.com/commerce/produc … ts_id=8745),
however, uses only 10k resistors and the BSS138 "N-Channel Logic Level
Enhancement Mode Field Effect Transistor", a device that I am unfamiliar
with and was only able to ascertain the name from the datasheet.
The schematic leaves me a tad confused, however; the part description
refers to the “RXI”, “RXO”, “TXI”, and “TXO” pins – which seems simple
enough – but the schematic shows instead “_LV” and _HV" pins.
If someone would be kind enough to indicate which pins of the logic level
converter need be connected where, in terms of the names seen on the
schematic, I should be able to complete my circuit design.