XCTU problem

Hello SparkFun Forum.

THE SYSTEM:

2 year old Dell “business” desktop

Windows 7 with all updates

2 x brand new XBee PRO S1

1 x SparkFun XBee Explorer Dongle

1 x SparkFun XBee Arduino Shield+Arduino UNO V3 programmed with “XBee_Remote_Control.ino” from the SparkFun Xbee Shield Hookup Guide

https://learn.sparkfun.com/tutorials/xb … 1426219622

XCTU – current version with compatibility mode set to Windows 7

THE PROBLEM:

Using the Serial Monitor and the XCTU Console (as in the Hookup Guide) everything seems to work OK

i.e. If I ask the “dongle XBee” to request the “Arduino Shield XBee” to read analog pin 0 “a0” it works (I have a LDR giving a varying voltage to Arduino pin A0).

But if I set the XCTU to send a repeating looped sequence of “a0” with 500uS delays it works for a couple of minutes then the XCTU console appears to freeze.

This often happens around 4000 to 5000 Rx bytes

The DIN and DOUT lights on the 2 XBees continue to operate which seems to suggest to me that they are still communicating. The top left hand Tx/Rx icon on the XCTU console has arrows going backwards and forwards indicating data transfer but the rest of the console is frozen.

See images.

http://imagizer.imageshack.us/v2/640x48 … UsLWNq.jpg

http://imagizer.imageshack.us/v2/640x48 … toKqNN.jpg

The only way to recover the situation is to close XCTU, remove the “dongle XBee” and start again.

I’ve reinstalled XCTU and swapped my first 2 XBee PRO for another new pair (I’d purchased 4 units) and still the same thing happens. …. What am I missing?

I’m actually in the same problem with the same type of test (Sending continuosly potentiometer value from Arduino+Xbee to the Computer+Xbee+XCTU)!!! Did you solve it? :smiley: :smiley: :smiley: