Hi all,
i’m testing Yagarto under XP/2000 to choose the IDE for the company.
I installed the three packages supplied by the site.
My problems are:
- on the original makefile i had a number of ‘echo’ commands to comment each operations: now i receive :
process_begin: CreateProcess(NULL, echo -------- begin --------, …) failed.
make (e=2): Impossibile trovare il file specificato.
I must comment out all the echo commands to compile.
- compiling a source i have:
arm-elf-gcc -c -mcpu=arm7tdmi -mthumb-interwork -I. -x assembler-with-cpp -DRAM_RUN -Wa,-adhlns=src/CStartup.lst,-gstabs src/CStartup.S -o src/CStartup.o
arm-elf-gcc -c -mthumb -mcpu=arm7tdmi -mthumb-interwork -I. -gstabs -DRAM_RUN -O2 -Wall -Wcast-align -Wcast-qual -Wimplicit -Wpointer-arith -Wswitch -Wredundant-decls -Wreturn-type -Wshadow -Wunused -Wa,-adhlns=src/main.lst -I… -MD -MP -MF .dep/main.o.d -Wstrict-prototypes -Wmissing-declarations -Wmissing-prototypes -Wnested-externs -std=gnu99 src/main.c -o src/main.o
src/main.c:44: warning: …
…
D:\DOCUME~1\xyz\IMPOST~1\Temp/ccqabaaa.s: Assembler messages:
D:\DOCUME~1\xyz\IMPOST~1\Temp/ccqabaaa.s:650: Error: can’t resolve main' {.text section} - main’ {.text section}
make: *** [src/main.o] Error 1
What does it mean? Of course the main function is not missing and the same source is compiled by other compiler…
Thanks !