Hi Scott & Paul,
OK… Some updates for you…
I started writing the GNSS SPI logger example and couldn’t get the GNSS to begin on SPI. I started looking back through the SPI examples I wrote a while ago and found this cryptic “note to self”:
https://github.com/sparkfun/SparkFun_u- … no#L42-L45
The SPI examples themselves are here:
https://github.com/sparkfun/SparkFun_u- … amples/SPI
I configured my SPI logging example so it would keep attempting to begin:
// Connect to the u-blox module using SPI port, csPin and speed setting
// ublox devices generally work up to 5MHz. We'll use 4MHz for this example:
bool begun = false;
do
{
begun = myGNSS.begin(SPI, GNSS_CS, 4000000);
if (!begun)
{
Serial.println(F("u-blox GNSS not detected on SPI bus. Please check wiring."));
delay(1000);
}
}
while (!begun);
I left that running while I connected to the ZED-F9P using u-center over USB.
I opened up “Messages View” and selected UBX \ CFG \ PRT (Ports).
I set Protocol In and Protocol Out to “None” on both 0-I2C and 1-UART1. (Click “Send” to apply each change.)
Still no joy.
I set Protocol In and Protocol Out to “0+1+5 UBX+NMEA+RTCM3” on 4-SPI…
Hey presto! The GNSS began and I could communicate with it.
So it appears that the SPI port needs a kick to enable the UBX messages / protocol.
I’ll try saving the configuration into BBR and see if I can still begin the GNSS after power-cycling it. It would be nice not to have to mess about with CFG PRT each time…! ![]()
I’ll post an update later.
I hope this gets you going!
Paul