Hi team,
I would increase the F9P update rate by setting the CFG-RATE via u-center. For example, if I would set 50ms (20Hz), should I need to update both the base device and rover device with the same one, or I should only need to update the base?
Also, according to the datasheet document of ZED-F9P, there are 3 rate parameters. The RTK update rate is up to 8Hz, PVT is up to 10Hz, and RAW is up to 20Hz in GPS+GLO+GAL+BDS mode. I am wondering if I set the CFG-RATE, which rate parameter will be updated? If the RTK rate will be updated, I couldn’t set the value lower than 125ms (8Hz), right?
I am using a PX4-based drone, and I tried to set CFG-RATE, but it seems PX4 will automatically rewrite my setting by default. Do you have any advice to stop PX4 rewriting?
Many thanks.
Yu