I am using the SparkFun ZED-F9R with dead reckoning and u-center version 24.05. Why can’t I configure settings in the Message View or Configuration View? I need to set them in the Generation 9 Advanced Configuration View for the changes to take effect such as rate
Also, when using the SparkFun ZED-F9R for calibration to enter Dead Reckoning mode, I need to drive for a while, and then I have to select the UBX-NAV-PVT menu before the status changes to 3D+DR GNSS. Why doesn’t it switch automatically, even though everything shows as calibrated, including the accelerometer and gyroscope?