Hi,
I’m trying to use ZX Distance and Gesture sensor (SEN-13162) which is placed behind the semi-transparent mirror (70% opacity). After making optical separation to avoidcrosstalk by stray light inside the housing between transmitters and receiver, the sensor can detect gestures but only with limited range (up to 7cm). Also Z coordinate is limited: ~240@7cm, ~70@1cm from sensor.
This seems like a problem due to mirror semi-transparency - received IR signal is weaker as expected by the microcontroller.
Could you please advise how to “calibrate” gesture sensor, so it can be used behind various semi-transparent surfaces like semi-transparent mirrors with increased range (~20cm)? It would be great to allow users to modify sensor parameters like:
-
Increase IR LED power / PWM freq (boost level)?
-
Change receiver sensitivity levels?
-
Modify PIC16F1823 firmware (I’ve noticed some undocumented pins on the top of the sensor)?
I’ve studies “GestureSense XZ01 Sensor I2C Register Map” but there is no option to “re-calibrate” it.
I love the sensor because of its design - IR transmitters and receiver are separated by enough free space, other IR sensors have those too close.
Also, XYZ version of the gesture sensor would be great (with swipe UP/DOWN gestures ![]()
Thank you for your ideas!