2.4" OLED Displays

There are some beautiful new OLED displays coming out that are about 2.4/2.8" wide – a really handy size. Here is a link below:

http://www.osddisplays.com/oled.php

Specifically, the OSD024AMQV-T (2.4", 320x240, and either RGB or SPI interface) looks amazing. I know Sparkfun has recently started carrying OLED screens with a high-level controller built in, but for some of us who prefer low-level interfaces, I’d love to see some OLED displays without the external controller, that were more economical.

thanks!

Me too :smiley:

A display with a low-level interface allows to send data faster than simple but slow serial-based display (I’m not talking about SPI displays, they are quite fast too, I’m talking about display+micorcontroller+115200 serial port)

And that display seems to have a controller chip with framebuffer, so it won’t be that difficult to use.

It would also be nice a cheap monochrome OLED

I would like on of them too.

A barebone LCD/OLED with a breakout board and I would buy one right away.

The serial interface is nice, but I want higher frame rates.

www.osddisplays.com OLEDs looks like the one 4dSystem is using. Do they have specifications available?

Edit:

Well we could always strip the controller from a 4dSystem AMOLED module as long as we have the specifications for the OLED pannel itself.

Or get the psp LCD and make our own breakout board, but that is a LCD not OLED so it get’s a -1 to the coolness factor. :roll:

The more I look at the specifications for these displays, the more I’d love to try one out!

Here’s another company that looks to sell displays similar to those at OSD:

http://www.vision-opto.com/C0283QGLF-T.htm

Their quick specifications sheet says the display uses the S6E63D6 controller, and a quick google came up with a datasheet:

http://www.cec-mc.ru/comp/lcd/powertip/pdf/S6E63D6.pdf

Really nice specs:

CONTRAST 1/10000(typ.)

BRIGHTNESS 200cd/m2

VIEWING ANGLE 170 degree

RESPONSE TIME 50uS

SIZE 2.83"

It’s nearly as big as the PSP LCD, but it has a framebuffer! so no fpga, sram and complex lcd controller :shock: this seems easily interfaceable with a simple microcontroller using parallel (or even spi) connection :slight_smile:

After mentioning I was just a graduate student, I haven’t had any luck with OSD displays. Initially they had said their minimum order quantity is 500, and they’re only able to support one order below that for development purposes. (But perhpas that only extends to non-students :slight_smile: ).

I’ve just sent an e-mail to vision-opto. Hopefully there will be more luck with them!

I agree, this display seems vastly more useful than the PSP LCD in that, even though it’s a little smaller, it contains both a framebuffer and some potentially easy-to-use interfaces. Imagine controlling such a beautiful LCD with nothing more than a small microcontroller over an SPI interface!

I haven’t had any luck in trying to obtain a small quantity of these displays :frowning:

perhaps we should light the bat signal and hope that someone from Sparkfun sees it and is able to begin to offer these beautiful looking displays relatively inexpensively in small quantities. :slight_smile:

We could just buy the 4d systems and strip the picaso controller, if we want low level access to the OLED.

As long as we find out what OLED modules they use and the specs for them.

$230 is a little much for a single 2.8" display – maybe something on the order of $50-75 would be okay.

silic0re:
After mentioning I was just a graduate student, I haven’t had any luck with OSD displays. Initially they had said their minimum order quantity is 500, and they’re only able to support one order below that for development purposes. (But perhpas that only extends to non-students :slight_smile: ).

I’ve just sent an e-mail to vision-opto. Hopefully there will be more luck with them!

I agree, this display seems vastly more useful than the PSP LCD in that, even though it’s a little smaller, it contains both a framebuffer and some potentially easy-to-use interfaces. Imagine controlling such a beautiful LCD with nothing more than a small microcontroller over an SPI interface!

I have had real bad luck with OSD-Displays. They do not even reply if they don’t think your going to have any quantity business. I have had much better success with US Micro Products http://www.usmicroproducts.com. They have very reasonable prices, and seem to be willing to sell 10’s of units (at a great discount from the sample price, it was about 50% for me).

Did you ever hear back from vision-opto?

Unfortunately I haven’t heard back from vision-opto. It doesn’t look like US micro products has OLED displays near 2.4/2.8" – I wonder if they might begin to carry them soon?

silic0re:
Unfortunately I haven’t heard back from vision-opto. It doesn’t look like US micro products has OLED displays near 2.4/2.8" – I wonder if they might begin to carry them soon?

They do actually I believe. They have some displays that are not on the web page. I asked them if they had any AMOLED displays (which they do not have listed) and they said yes they do and sent me the data sheet for one.

I would call and ask, they are very good on the phone.

Mike

b_bogk77:
We could just buy the 4d systems and strip the picaso controller, if we want low level access to the OLED.

As long as we find out what OLED modules they use and the specs for them.

I think $230 qty of 1 is fine for display prototyping, especially if you want that cool display controller. Obviously if you went into production with something, costs would be quite low – even if you oem’ed the picasso controller.

Those bare OLED screens are cheap… now finding a supplier :slight_smile:

maokh:
I think $230 qty of 1 is fine for display prototyping, especially if you want that cool display controller. Obviously if you went into production with something, costs would be quite low – even if you oem’ed the picasso controller.

Those bare OLED screens are cheap… now finding a supplier :slight_smile:

I think the point of finding someone that sells the bare displays is that its cheaper even in prototype quantities. At least 5 times cheaper if you go by that $230 figure. In fact, I can buy almost 10 of the 160x128 displays I am building a prototype with for that price… Most people that want a bare display aren’t going to care about the Picasso controller, so its just an extra expense.

The device I am prototyping has to be as thin and as low power as possible, (which is why I went OLED in the first place) so the Picasso controller would just be an extra drag on the system, and the assembly itself looks to be thicker then my goal of 6-7mm, so its definitely a no go for me.

Its definitely a neat little device for the PIC and AVR ppl that just want a simple serial interface though :slight_smile:

I have a lead on 2.0" AMOLED from a distributor here in Hong Kong. I believe they also carry other sizes, but I am most interested in the 2.0" (176x220 resolution) without touch screen.

I am considering buying the displays to sell through www.Brilldea.com, but before I drop the cash for it I wanted to see if there was interest. AMOLEDs are not cheap, not yet, so the selling price I was thinking was US$59.95/display. This is just the display, no additional high level controller, only the glass, FPC and local controller (HX5051-A).

almost there! :slight_smile:

http://cogsci.mcmaster.ca/~peter/notes1 … -small.jpg

I only had an hour or so to hack out some quick test code – I think I can successfully write to the registers, because I can ‘turn on’ the display, and take it out of standby, etc., but haven’t been able to successfully draw actual pixel data to the screen just yet. I’m writing to the framebuffer, but for some reason it’s not displaying, and I haven’t had a great deal of time to debug just yet. :wink:

you might want to tell us a bit more about the display, what model? where did you got it, cost, etc…

With only that small picture there is nothing interesting here :slight_smile:

Sorry :slight_smile: I didn’t want to say too much until I have something definitely working.

The display is the 2.8" OLED from OSD displays, although I am fairly convinced that the displays from vision-opto, OSD, (and the one used by 4D systems) are the same display(s).

From what I gather, the displays from OSD cost about the same as from vision-opto ( viewtopic.php?t=10550&highlight=oled ), about $30. OSD was kind enough to let me order a couple as a sample order, and they arrived the next day!

The breakout board for the display’s connector was milled on a PCB mill, and just breaks out all of the connectors pins. In terms of interfacing, the display requires about 15 external capactitors, ~3v, ~4.6V, and -4.4v. Other than that, the interface looks very straight forward: either parallel (16-bit), or SPI. The 16-bit interface isn’t a standard address/data interface – you use the same pins for data and address (sort of), in that the data you send is either interpretted as setting an instruction address or writing data depending on the status of an ‘instruction register or RAM’ pin (if that makes any sense). I hope to tinker with the parallel interface after the SPI is working and I can get an idea on the framerates possible with SPI.

The OLED display is very, very bright – even with just the garbage on the display I’m getting so far, it’s obvious that it’s a very bright and high contrast technology. I had no idea, and thought the pictures of the 4D systems displays were in some way manipulated or the result of creative photography. The displays are really that bright and high contrast.

pretty cool :slight_smile:

WOW :smiley:

Any chance sparkfun might stock those displays?

ChiMei have come up with a 4.3in diagonal AMOLED…

http://www.glyn.co.nz/Displays_CMEL.htm

I’ll contact GLYN and see how much they are…