From your comment that the note on the schematic is for coin cell (or at least, not for 3.7 V LiPo battery connected to the Artemis’ LiPo charger), is it then true that
the 3.7 V LiPo connected to the Artemis’ charger will operate the Redboard Artemis without problem?
Then the second question,
How can a single battery be connected to power several Redboard Artemis units?
Unfortunately, there is not a LiPo charger on this board.
The modules could be connected to the same Coin Cell battery but all the other components may pull too much current to support multiple boards on one Coin Cell. So connecting several boards to the same Coin Cell is not advisable.
I goofed…looking carefully on the schematic for the Redboard Artemis, DEV-15444, it shows (alongside the batttery) CR2032.
Now, re LiPo Charger, going to the Arduino Comparison Guide (Advanced), the Redboard Artemis, DEV-15444 is the first board shown. It has “LiPo Charger Yes”
That’s my currrent question - what does “LiPo Charger Yes” mean, in the Arduino Comparison Guide?
Thank you for bringing that error to my attention. Only one out of the three Artemis boards has LiPo charging, the [Artemis Nano. I have alerted our teams to fix this error.
I had not read the Redboard Artemis schematic carefully…thanks for straightening me out.
Then the remailing question - can the 3.7 V LiPo btteries be used to power the Redboard Artemis without a problem? If so, what pin would the 3.7 V LiPo be connected to?
The general higher voltage input goes through the separate connector, “VIN range 5-15V”. So the LiPo batteries are below the minimum voltage required there.
At this point, I would recommend not using a LiPo battery unless you can add supplemental circuitry to meet the current power requirements for this particular board.
Brandon is correct on the supplemental circuitry : Looking at the schematic off the board , the VBATT is connected with a diode to 3V3 generated on the board. If you put a diode serial with the PLUS(+) from 3.7V LIPO and connect the other side of the diode to the 3V3 on the connector, you will feed the board with ~3V ( and diode typically takes 0.7V). The diode does not need to be a heavy one, 1N4001 or so will do. The LIPO will not be charged of course (given the diode).