I am attempting to read voltage levels from the ADS1015 by connecting it through Qwiic cables to an OpenLog Artemis, which is returning “Known I2C address but device failed authentication at address 0x48” and will not recognize the ADC. This part is listed as supported on the Openlog Artemis so is there anything that can be done? The OpenLog seems to work correctly with the Qwiic scales I have purchased as well as the internal IMU. I read in a thread that I can no longer find that it might not be recognized if there is no voltage input on the ADC, so I tried resetting it with both 3.3V on A0 and 2.5V differential A1/A0. The problem persists weather or not I use a Mux, the serial output just repeats the error more frequently.