I recently received a SEN-15577/A111 60 GHz. pulsed radar board. I plugged it into a Raspberry-Pi-3 and then I downloaded and unzipped the SDK from github (SparkFun_Pulsed_Radar_A111_Example_Code-master.zip). At first I had trouble with compilation errors, but that was resolved by going to the most recent version of Raspbian (raspbian-buster). I now can make the execuatibles but they don’t seem to run. {Note: I did edit /boot/config.txt to enable SPI}. The console log below illustrates my problem.
What am I missing?
############################################ Console log ###########################################
# Login @ Sat Oct 19 14:55:33 EDT 2019 in "/Users/wellsca/Desktop"
# Last deh_get @ Fri Jun 22 18:23:10 EDT 2018
[/Users/wellsca/Desktop]$ rpi
# ssh 10.0.1.21
Linux raspberrypi 4.19.75-v7+ #1270 SMP Tue Sep 24 18:45:11 BST 2019 armv7l
The programs included with the Debian GNU/Linux system are free software;
the exact distribution terms for each program are described in the
individual files in /usr/share/doc/*/copyright.
Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent
permitted by applicable law.
Last login: Sat Oct 19 19:44:15 2019 from 10.0.1.7
wellsca@raspberrypi:~ $ gcc --version
gcc (Raspbian 8.3.0-6+rpi1) 8.3.0
Copyright (C) 2018 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
wellsca@raspberrypi:~ $ cd wd/A111/
wellsca@raspberrypi:~/wd/A111 $ ls -l
total 60
-rw-r--r-- 1 wellsca wellsca 47791 Sep 30 17:51 5768487.pdf
drwxr-xr-x 4 wellsca wellsca 4096 Sep 26 18:54 SparkFun_Pulsed_Radar_A111_Example_Code-master
drwxr-xr-x 5 wellsca wellsca 4096 Oct 17 01:49 unzipped
drwxr-xr-x 2 wellsca wellsca 4096 Oct 11 21:39 zipped
wellsca@raspberrypi:~/wd/A111 $ ls -l zipped/
total 24168
-rw-r--r-- 1 wellsca wellsca 10858538 Oct 11 21:23 A111_Pulsed_Radar_Breakout-master.zip
-rw-r--r-- 1 wellsca wellsca 4753245 Oct 9 18:41 SparkFun_Pulsed_Radar_A111_Example_Code-master.zip
-rw-r--r-- 1 wellsca wellsca 9127830 Oct 9 18:40 SparkFun_Pulsed_Radar_Breakout_A111-master.zip
wellsca@raspberrypi:~/wd/A111 $ cd SparkFun_Pulsed_Radar_A111_Example_Code-master/Acconeer\ SDK/acconeer_rpi_xc111_v1_8_6/rpi_xc111/
wellsca@raspberrypi:~/wd/A111/SparkFun_Pulsed_Radar_A111_Example_Code-master/Acconeer SDK/acconeer_rpi_xc111_v1_8_6/rpi_xc111 $ make clean; make
Compiling example_service_power_bins.c
Compiling acc_driver_spi_linux_spidev.c
Compiling acc_driver_gpio_linux_sysfs.c
Compiling acc_driver_hal.c
Compiling acc_driver_os_linux.c
Compiling acc_device_os.c
Compiling acc_device_spi.c
Compiling acc_device_gpio.c
Compiling acc_log_integration.c
Creating archive libcustomer.a
Compiling acc_board_rpi_xc111_r4a_xr111-3_r1c.c
Linking example_service_power_bins_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
Compiling example_detector_motion.c
Linking example_detector_motion_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
Compiling example_detector_obstacle.c
Linking example_detector_obstacle_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
Compiling example_service_envelope.c
Linking example_service_envelope_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
Compiling example_detector_distance_peak.c
Linking example_detector_distance_peak_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
Compiling example_detector_distance_basic.c
Compiling acc_detector_distance_basic.c
Linking example_detector_distance_basic_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
Compiling example_service_iq.c
Linking example_service_iq_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
Linking acc_streaming_server_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
Compiling acc_service_data_logger.c
Linking acc_service_data_logger_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
Compiling example_service_sparse.c
Linking example_service_sparse_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
wellsca@raspberrypi:~/wd/A111/SparkFun_Pulsed_Radar_A111_Example_Code-master/Acconeer SDK/acconeer_rpi_xc111_v1_8_6/rpi_xc111 $ cd out/
wellsca@raspberrypi:~/wd/A111/SparkFun_Pulsed_Radar_A111_Example_Code-master/Acconeer SDK/acconeer_rpi_xc111_v1_8_6/rpi_xc111/out $ ls -l
total 5456
-rwxr-xr-x 1 wellsca wellsca 666792 Oct 19 19:58 example_detector_distance_basic_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
-rwxr-xr-x 1 wellsca wellsca 717848 Oct 19 19:58 example_detector_distance_peak_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
-rwxr-xr-x 1 wellsca wellsca 778952 Oct 19 19:58 example_detector_motion_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
-rwxr-xr-x 1 wellsca wellsca 859880 Oct 19 19:58 example_detector_obstacle_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
-rwxr-xr-x 1 wellsca wellsca 657544 Oct 19 19:58 example_service_envelope_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
-rwxr-xr-x 1 wellsca wellsca 762524 Oct 19 19:58 example_service_iq_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
-rwxr-xr-x 1 wellsca wellsca 632496 Oct 19 19:58 example_service_power_bins_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
-rwxr-xr-x 1 wellsca wellsca 484652 Oct 19 19:58 example_service_sparse_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
drwxr-xr-x 2 wellsca wellsca 4096 Oct 19 19:58 lib
drwxr-xr-x 2 wellsca wellsca 4096 Oct 19 19:58 obj
wellsca@raspberrypi:~/wd/A111/SparkFun_Pulsed_Radar_A111_Example_Code-master/Acconeer SDK/acconeer_rpi_xc111_v1_8_6/rpi_xc111/out $ ls -l /dev/spi*
crw-rw---- 1 root spi 153, 0 Oct 19 19:11 /dev/spidev0.0
crw-rw---- 1 root spi 153, 1 Oct 19 19:11 /dev/spidev0.1
wellsca@raspberrypi:~/wd/A111/SparkFun_Pulsed_Radar_A111_Example_Code-master/Acconeer SDK/acconeer_rpi_xc111_v1_8_6/rpi_xc111/out $ sudo ./example_detector_distance_basic_rpi_xc111_r4a_xr111-3_r1c_a111_r2c
Acconeer software version v1.8.6
Acconeer RSS version 1.0
00:47:21.310 [ 1601] (E) (sensor_protocol): Timeout waiting for indication on sensor 1
00:47:21.310 [ 1601] (E) (cpd_cbank_calibration): Failed to retrieve indication.
00:47:21.310 [ 1601] (E) (cpd_cbank_calibration): Failed to get CBank result.
00:47:21.310 [ 1601] (E) (sensor_manager): calibrate_sensor: Sensor control: Calibration failure for sensor 1
00:47:21.310 [ 1601] (E) (detector_distance_basic): Distance basic detector not possible to create
acc_detector_distance_basic_create() failed
wellsca@raspberrypi:~/wd/A111/SparkFun_Pulsed_Radar_A111_Example_Code-master/Acconeer SDK/acconeer_rpi_xc111_v1_8_6/rpi_xc111/out $