Accuracy TAS606 load cell

Hi all,

I need to measure relatively high weights reaching up to 200 Kg. It must be accurate within +/- 5 kg.

Currently I found a pancake load cell (TAS606) which specifies it can reach up to 200 Kg, but I cannot find additional information in regards the accuracy.

I would like to know if there is someone who has more information on the max accuracy.

And I would also like to know any further experiences with this device, please let me know!

Kind regards,

Imre

Hello

For me I have not interacted with the TAS606 load cell but i can offer a solution with the best load cell that i used in doing such a project in the past. Use FC23 compression load cell. See the link https://www.te.com/commerce/DocumentDel … ng=English

to find the datasheets and how to integrate it into your system. It has a maximum loading of 226 Kg and very high accuracy