I have a TAS606 Disc type load cell that I am using, however I am having some issues with it. I have the 200 kg rated load cell, and it is reading very well up to 10 kg, however after this point the load cell does not read accurately. The load cell has never read above 20 kg, despite 200 kg being applied to it. Are there any calibration settings that I need to be aware of? Do you know how I could fix this issue?
brow
2
Please see here:
Related topics
| Topic | Replies | Views | Activity | |
|---|---|---|---|---|
| Support for Load Cell - 200kg, Disc (TAS606) | 2 | 42 | March 24, 2025 | |
| Load Cell - 200kg, Disc (TAS606)... is it really 200kg? | 2 | 933 | October 28, 2019 | |
| Accuracy TAS606 load cell | 1 | 707 | November 27, 2021 | |
| TAS606 max weight before damage | 3 | 1790 | April 11, 2023 | |
| configuration Load Cell - 200kg, Disc (TAS606) with HX711 | 2 | 803 | October 25, 2021 |