configuration Load Cell - 200kg, Disc (TAS606) with HX711

I would like to know if the load cell (tas606 - 200 kg) is compatible with the amplifier HX711. and if 4 load cell could be connected to the same hx711.

Yep! That’s exactly how it’d designed to function - be sure to run through the hookup guide here that will walk you through the steps involved https://learn.sparkfun.com/tutorials/lo … 1615791300

Hi there,

I have used the OpenScale successfully with 6 and 10Kg load cells (from CAS) - calibration factor kind of 400 to 700.

When i try bigger cells, 100Kg, 200Kg the calibration factor is so low (20 - 40) that every increment moves so many grams I can’t get it accurate.

Is there a way to have finer precision to the calibration settings?