I need to find a ADC that goes from 0 to 10V… 8 to 12 bits of resolution… Output fed to pins not bit stream… not exactly what is needed. Does sparkfun or someone has one?
Hi zzzones and thanks for posting,
I do not think SparkFun will have an [ADC that matches what you are looking for. The only dedicated ADC’s SparkFun carries are the [MCP3002 and the [Qwiic 12-Bit ADC (ADS1015) and both of these have a max input of ~5.5V for your analog input voltage. You could use a voltage divider for your analog input but that may not work for your application depending on how accurate you need it to be.
I am not sure where you might find an ADC that would match your criteria, unfortunately. You could try checking with a larger distributor like Mouser, Digi-Key or Jameco.](SparkFun Qwiic 12 Bit ADC - 4 Channel (ADS1015) - DEV-15334 - SparkFun Electronics)](Analog to Digital Converter - MCP3002 - COM-08636 - SparkFun Electronics)](ADC / DAC - SparkFun Electronics)