Hi,
I’ve recently acquired one Adjustable Lipo Charger PRT-14380 from one of your retailers.
After trying to charge a 800 mAh lipo (just in case, the lipo health was good) at 300 mAh which took more than 12h (disconnect before charge ends, and only 0.2-0.3 V raised), i’ve devided to make some tests.
Stuff used :
I tried with different li-ion battery :
All listed batteries - but the 50 mAh Lipo & the coin cell - can handle at least 500 mAh charging current (tested with another charger).
For each battery, I’ve tested all the presets switches (except for the smallest ones).
With the 100 mAh switch, charging current was about 16 mAh, according to the DMM.
With the 200, 300, 400 and 500 mAh switches, it was about 7 mAh.
With a 68k Ohms resistor and the PTH switch, I got about 14 mAh, which is - according to the ~15 mAh theorical minimal current - fairly good, but I think it’s much more a coincidence.
First, I thought it was the termination current, but most of the batteries were only half charged, or empty, so I’m pretty sure it wasn’t.
Second, I thought it was preconditioning, but after 15 minutes of charge and same current, it wasn’t.
One important thing is that I let the LIR2450 coin cell charging totally (PTH switch, 68k resistor). It took time, but it was ok.
Same for the 50 mAh lipo.
So, for sure it can charge a battery, but current is wrong.
I’ve also tried :
Also, I’ve noticed that :
I can’t figure out what’s wrong.
I’m pretty sure I didn’t short-circuited or damaged anything.
I’m charging only one battery at a time, and only one switch is ON.
No strange smell while using it, and resistors didn’t heat. Nothing looks strange when looking at the circuit board.
Supply voltage is good, charger output voltage seems to be acceptable too (~4.31V with no load), and when I’ve plugged a battery, the blue led turned ON and the battery started charging.
Of course when a full (4.2V) battery was plugged, the blue led stayed OFF.
So, the behaviour seems to be normal.
Could it be a circuit fault ? Or anything else I’ve missed ?
I’ve mailed the retailers but no answer.
I’m not hardly looking for a guarantee, but I wanna know if it’s more a bad use or a factory default.
Best regards,
Christophe