ADUC Jtag and OpenOCD

Hi

I want to use openpcd ad debugger for aduc70xx uCs.

OS is Windows XP.

I use the jtag adapter which is part of the aduc7026 evaluation board.

It should be the same as the amortec jtag interfaces (mIDAS-Link, RDI).

In devicemanager it es recognized as “J-Link”

Does anybody know I can use this device?

When I try to use it I get this error:

C:\CrossSampleLess>openocd-ftd2xx -f arm7_ft2232.cfg

Info: openocd.c:93 main(): Open On-Chip Debugger (2007-09-05 09:00 CEST)

Error: ft2232.c:1341 ft2232_init_ftd2xx(): unable to open ftdi device: 2

Next question: Hoy do I have to setup the cfg file to work with an aduc? I

only see options for lpc controllers. I read in the forum some people where

able to run openocd with aduc but I don’t know how they made it.

I read flash debugging id not possible with aduc7000 uCs. Is this still true?

Thanks for your help,