AI Cannot Be Trusted - @GDT is right, here's what SWMAPS, Grok, Claude, Google AI and ChatGPT said about the exact same data

I believe @gdt is correct, AI seems to be a lot of malarky……

Prompt was - What is the distance from (PT31) 35.685188890 -84.566496030 to (PT33) 35.683247975 -84.566380047 to (PT36) 35.682953718 -84.565805490 to (PT15) 35.676522981 -84.570140749

In SW MAPS the Measure Tool reports (All points were RTK FIX LAT/LON)

PT31 to PT33 707.369ft
PT33 to PT36 201.365ft (BTW I measured this with Tape and attempting to compensate for elevation changes using up more tape, I am pretty sure this is 201.x ft.
PT36 to PT15 2,671.689ft

Here’s what AI’s had to say
Grok said (Elon for the win ?!?!?)
Segment distances:
PT31 → PT33
: ≈ 216 m (709 ft)
PT33 → PT36: ≈ 61 m (201 ft)
PT36 → PT15: ≈ 815 m (2,675 ft)

Google Web search AI Mode
The segment-by-segment breakdown is as follows:
PT31 to PT33: ~706 feet (0.13 miles)
PT33 to PT36: ~201 feet (0.04 miles)
PT36 to PT15: ~2,693 feet (0.51 miles)

ChatGPT said
PT31 → PT33 Meters: ≈ 216.0 m Feet: ≈ 708.6 ft
PT33 → PT36 Meters:
≈ 57.6 m Feet: ≈ 189.0 ft
PT36 → PT15 Meters:
≈ 825.6 m Feet: ≈ 2,708.6 ft

CLAUDE AI said
PT31 to PT33: Distance: approximately 715 feet
PT33 to PT36:
Distance: approximately 215 feet
PT36 to PT15:
Distance: approximately 2,850 feet

Perplexity said
Using great‑circle (haversine) distance on WGS‑84, the segment distances are approximately:​

PT31 about 0.13 miles ≈ 710 ft.
PT33 about 0.04 miles ≈ 200 ft.​
PT36 about 0.46 miles ≈ 2,420 ft.​

I will need to try out @Andrew74 ‘s new Tool he’s testing at the link…. I am getting great RTK FIX with new PointPerfect RTCM/NTRIP compared to PointPerfect MQTT (eoL Fall 2026), but now I am pondering what is right for my validation of Survey Pins to field measurements. Maybe GROK is pretty good….??

And in going with GROK for the win I asked below…..
FYI the deed measurements I am working on validating are 708.22ft, 201.47ft, 2,677.76ft I am trying to set flags to be close before I spend 20-30 minutes at each point getting very best readings, instead I did about 5 minutes per point (Setup, level Surveyors pole, let GPS settle for 1-2 minutes, then take a 60-80pt average reading)

Prompt to GROK – can you repeat those calculations out to the full reported decimal places in the Latitude and Longitude as I took the readings with a SparkFun RTK Torch with RTCM/NTRIP corrections, and report the results in feet out to two decimal places please?

Here are the straight-line (great-circle) distances calculated using the full reported decimal places from your SparkFun RTK Torch readings (with RTCM/NTRIP corrections for high accuracy). Results are shown to a much higher precision internally, but reported here with meters to 4 decimal places and feet to 2 decimal places as requested.

Individual segment distances:

  • PT31 (35.685188890, -84.566496030) → PT33 (35.683247975, -84.566380047) ≈ 216.0740 meters / 708.90 feet *Chris Comment - Deed 708.22ft

  • PT33 (35.683247975, -84.566380047) → PT36 (35.682953718, -84.565805490) ≈ 61.3474 meters / 201.27 feet *Chris Comment - Deed 201.47t

  • PT36 (35.682953718, -84.565805490) → PT15 (35.676522981, -84.570140749) ≈ 815.2586 meters / 2674.73 feet *Chris Comment - Deed 2,677.76ft

Total path length (PT31 → PT33 → PT36 → PT15):
≈ 1092.7 meters (1.093 km)
≈ 3584.91 feet (≈ 0.68 miles)

These are precise “as the crow flies” distances using the haversine formula and the WGS84 Earth model (mean radius ≈ 6371 km). With RTK-level coordinates like yours, the positional accuracy is typically in the centimeter range, so these distances should be very reliable for most practical purposes. If you’re following an actual ground path (trail, road, boundary, etc.), the real-world travel distance will be somewhat longer.

Let me know if you need any other units, bearings/azimuths between points, or further analysis!

You have established that LLMs are bad at math. So just stop trying to use them. Asking others to think about LLM output is impolite.

T-800 has entered the chat.

Sorry @gdt I thought it was interesting to show what the AI’s produced, as many people out side the SparkFun Community use them for a lot of things, and it proves what you had mentioned in an earlier thread, they can be wildly incorrect. Since I don’t have a background in surveying, and harvest lumber for a living, I have to rely on the imperfections of AI to some degree to learn. Please take no offence from my posts, I am sorry it was impolite of me to @ you . I won’t do it again (@ you) Please have a great day. Chris

Exactly…. we are all dead, but perhaps their shooting will be as accurate as Stormtroopers if they are using AI for their calculations on aiming!!!

i agree, you can’t trust AI output.

For me it’s useful as a brainstorming tool, but not as a source of truth. In many situations AI helps with a Novel approach to a problem since it doesn’t mind making wild suggestions. But you need to be knowledgeable “enough” in the subject to weed out the stupid ones. So for me AI is helpful……sometimes :face_with_peeking_eye:
But it’s usually extremely frustrating during the process.

yes, I have at least learned enough to see when it’s calculations are crazy, but it has helped me learn so for me as a NON-Surveyor, technical farmer, it is helping me understand the flaws and the adjustments. Overall it’s helpful, but you need to learn enough to spot when it is off the rails CRAZY!!!

I would suggest getting a surveying textbook and reading it. That’s what I’ve done and it’s helped a lot.

I have not read this one but you can get a pdf at no charge, and the authors are faculty.

In particular it will talk about coordinate reference systems. That’s very important to understand.

My other advice is to learn to use QGIS. Being able to bring all your observations, plans and other data into a common view with background imagery is really useful.

Thank you for that link, adding it to my tablet for reading now!!!

I wrote a small desktop application while I was working at Garmin in the Automotive OEM group. I used it to convert between different position representations, and to estimate distances. I used it a lot while developing Point Of Interest search while we were developing in-dash navigation for Daimler. Daimler required that we use maps in NDS (Navigation Data Standard) format – a map format developed by a consortium of European auto makers. Map data were represented using a tiling scheme at multiple resolutions.

I needed a fast way to estimate distances based on Morton Code. My search code used an approximation based on great-circle distance on a spherical Earth. I converted lat/lon to unit vectors and used the squared magnitude of vector cross products to calculate relative distances for sorting by distance. A few more calculations were need to get the final great-circle distance.

For precise WGS 84 geodesic distance, I found GeographicLib (https://geographiclib.sourceforge.io/).

The screens shot shows 707.369 feet using GeographicLib and 709.699 feet using the approximation.

GeographicLib calculation are on the surface of the geoid. Height is not considered.