Alternative PCB thickness from batchPCB

does batchPCB (not another company) is currently supporting other board thickness (like 0.8 mm)

thanks

Have you checked the web site?

Yes and it say only 1.6 mm

But I already got from them smaller via board than it written there

Don’t want to sound rude but simple yes/no answer from someone that knows will do the work

Thanks anyway

If they say 1.6mm, then I think you have your answer. Plus, even if they did offer other thicknesses, I’m not sure I’d want to wait for them to fill up a panel. Why not just go with a place like Seeed Studio or Itead that offer different thicknesses, and are also cheaper?

thanks

I will try Seeed Studio

ITead might be better, I’ve used them for three lots of boards. They use the same factory as Seeed, but seem to deliver the boards quicker, and people appear to have fewer problems with them.