Can you do XYZ thickness, copper weight, solder mask color?

The short answer is no.

These orders are batched onto one panel. Everyone on that panel gets the same type board of course. So if you can find enough friends that want a certain setup, let us know. 100 square inch minimum.

If you have a single design that needs special consideration, and you could use 100 square inches, let us know. We will quote you a panel.

If you need 30,000 square inches, we can quote you large batches as well.

Possible thicknesses:

0.5mm 0.8mm 1.6mm 2.0mm 2.5mm 3.0mm

Available solder mask colors:

Red, Green, Black

Email pcbquestions@sparkfun.com for quotes.

Hmm. I’d really like to see a thinner board as a standard option.

0.062 is pretty thick, ESPECIALLY for the small boards where this

service is particularly attractive.