No, I want it for golf. A number of golf apps use cell phone gps for measurement. If the gps could give reliable location. 1-2m,
I could get rid of my laser range finder. Most golf apps have the ability to track shots, even putting distances. If the gps is wondering, you will not get good statistics. 1m would be pretty darn good, 2m would be sufficient.
What’s the difference between mikroe gnss 7 click and the Neo m9n break out board?
Same gps module but put on a different manufacturers board.
Built on the ESP32 WROOM usb C. Is there a better option?
That should do the job and it has a qwiic connector making it easy to connect the GPS. Keep in mind you will need to write a small program to read data from the GPS and spit it out over bluetooth.
Thanks for the reply. Helps me out, I’m understanding the products more. I’m thinking of taking a coding class to further learning all this stuff.
I did forget to mention that it’s meant to be a wearable. Therefore I was leaning towards the flat Molex Flexible GNSS Antenna - U.FL. Ideally mount the boards under the brim of a hat, 3D print an open air mount, Mount the flat antenna on the top.
Have you considered simply purchasing any one of a number of small GPS receivers that are designed to provide higher accuracy GPS/GNSS locations to phones and tablets?
Eg perhaps the Bad Elf Surveyor? You could attach it to your hat. It sends location data to your phone’s OS via bluetooth. The OS provides that improved location data to all the apps running on your phone.
Thought the new phones are pretty accurate these days.
EDIT: Oh, just saw that you want to build your own. Sounds like a fun project!
I ended up buying the Neo m9n u.fl and the Esp32 wroom usb-c.
I did get the Neo m9n to work directly thru my usb-c cable with u-center and u-blox. Hooked usb directly to Neo m9n. And I got NMEA data, sat info, etc.
I followed the hook up guide using qwiic connector to connect to the Esp32 wroom to the Neo m9n and it wouldn’t work. Are there tutorials on how to interface these two items and eventually get the Neo m9n data to get to my android phone via blue tooth and replace my cell phone gps with Neo m9n data using mock location?