The Anaren Air module is a small form factor RF Radio module with approx 6mm x 16mm footprint. They are SMT and impossible to solder leads directly to (I tried). They can be had with an on board trace antenna or a ufl connector.
They are based around the TI CC1101 chip and are available in 433,868,915 or 2.4. They communicate via SPI and have separate on board 64byte TX and RX buffers. They handle all packetization for you including preamble and checksum. They also have a Wake on Radio function.
The module can be had for $12.50 through Arrow. Digikey has them but they are much more expensive over there.
I had almost convinced myself that I was going to have to make a breakout board when I came across what TI calls a booster pack. You can only get these directly through TI but you get 2 Air modules mounted on what is essentially a protoboard with places for a switch, a uprocessor and a blank pad area in the middle for other components. These are designed to be used with one of TI’s development kits but they will work standalone. The beauty of this arrangement is that you get two modules on boards for $19.00. Plus the documentation has all of the register settings needed to get this thing up and running quickly. The kit actually comes with two uprocessors but they are MSP and I don’t want to use them personally. The boosters are based around the CC110 instead of the CC1101. The only difference I have been able to discern is the lack of Wake on Radio.
I ordered one of these last night. I will use this thread to keep up with my progress. I am hoping that this might encourage the hobby community to consider these as a low cost, tiny form factor alternative to the Xbee. They are not quite as plug and play but I needed the form factor more than anything else for my project.
I am also hoping that Sparkfun will consider picking these up and selling them on a breakout!
Here is a link to the booster pack https://estore.ti.com/430BOOST-CC110L-C … P2734.aspx If you follow the link back to Anaren, there is more detail about the board itself.