Aperture Problem With LFCSP16

So, I have a board with a bunch of devices, including an Analog Devices ADXL330, which has the footprint of the LFCSP16. The board kept getting aperature errors, which i finally narrowed down to the ADXL330. The error reported is that there was an aperature that was too thin (.0028").

I checked the pads for the LFCSP16 in the spec sheet, which are thin, but not that thin — .30x.50 mm.

The pads in the package design are .01378" x .027559" — I suspect this error reported (.0028") is the pad length which is too thin? But, .027559" is 27.599 mil, so that can’t be a problem, can it?

But, clearly I’m stabbing in the dark — the aperature that is too thin is reported as .0028", and the pad is .028"…so, what the frack? The LFCSP16 is small, but none of its dimensions are onthe order of .0028"

I tried just laying out a board only with this device, and still got an error. Then I tried — just for laughs — making a new variant of the device with my own package, and still got the errors. Then, I made the pads of my own package bigger and spaced them out…still, the error.

Any clues, please?

Julian

Julian,

I had the same problem last night when I was submitting a design.

I found the problem to be text I had placed on the copper pour.

The letters were to narrow, which I know for sure passed the last time I ordered.

If you have any text on the board (in copper) raise their size to 70 and ratio to 12, that will get their width high enough to pass.

If it isn’t a text problem, then Dave will have to point you in the right direction.

James L

Yeah, you know — I thought that might’ve been an issue, and I did have letters in copper on top, but I took that out and it still failed. I tracked it down to this particular part by mirroring each part, one by one, until the failure occured on the bottom of the board rather than the top.

But, now I’m not 100% sure why this particular part is having this aperature problem. I’m going to try and make my own package working from the device spec and see how that goes. I’ve verified that a trivial part with two SMD pads the same size as those for this particular device pass the DRC just fine — no aperature problems.

A bit confused…

Julian

Julian,

Dave might have to chime in here, there may be a problem with the bot, I can’t say for sure…

Maybe he will happen by soon,

James L

Emailing me usually works best ;). I was having too much fun with the board on my desk to check the forum.

What was the order name?

Cheers,

–David Carne

David…always playing…

Hey since you are checking the forum…atleast on this thread…when you guys going to get the pasted boards and the solder stencil option?

James L

David,

I’ll email you directly with a .zip of the Gerber files in question — but…the file upload never got so far as to actually place an order. I got this aperature error before I even got to the page where you select what CAD software was used.

Julian

Ah!

Yes, please email me with a zipped gerber.

propellanttech: Playing = designing cool stuff for the store ;).

Regarding stencils - the code is there, we’re still looking for a fab.

Not sure what you mean by “pasted boards”.

Thanks,

– David Carne