Arduino lilypad USB+bluetooth mate

Hi everyone, I bought an [Arduino Lilypad USB and a [bluetooth mate silver and I want my arduino to send datas to my Android phone (One plus one) through bluetooth. For this I’ve tried the program form sparkfun,

/*
  Example Bluetooth Serial Passthrough Sketch
 by: Jim Lindblom
 SparkFun Electronics
 date: February 26, 2013
 license: Public domain

 This example sketch converts an RN-42 bluetooth module to
 communicate at 9600 bps (from 115200), and passes any serial
 data between Serial Monitor and bluetooth module.
 */
#include <SoftwareSerial.h>  

int bluetoothTx = 11;  // TX-O pin of bluetooth mate, Arduino D2
int bluetoothRx = 10;  // RX-I pin of bluetooth mate, Arduino D3

SoftwareSerial bluetooth(bluetoothTx, bluetoothRx);

void setup()
{
  Serial.begin(9600);  // Begin the serial monitor at 9600bps

  bluetooth.begin(115200);  // The Bluetooth Mate defaults to 115200bps
  bluetooth.print("$");  // Print three times individually
  bluetooth.print("$");
  bluetooth.print("$");  // Enter command mode
  delay(100);  // Short delay, wait for the Mate to send back CMD
  bluetooth.println("U,9600,N");  // Temporarily Change the baudrate to 9600, no parity
  // 115200 can be too fast at times for NewSoftSerial to relay the data reliably
  bluetooth.begin(9600);  // Start bluetooth serial at 9600
}

void loop()
{
  if(bluetooth.available())  // If the bluetooth sent any characters
  {
    // Send any characters the bluetooth prints to the serial monitor
    Serial.print((char)bluetooth.read());  
  }
  if(Serial.available())  // If stuff was typed in the serial monitor
  {
    // Send any characters the Serial monitor prints to the bluetooth
    bluetooth.print((char)Serial.read());
 
  // and loop forever and ever!
}

I can received datas from the phone on the computer(not those I want to but anyway), but I can’t send datas frome the computer to the phone through the arduino. Can you help me please, it’s for an exam and you’re my only hope?](https://www.sparkfun.com/products/12576)](http://arduino.cc/en/Main/ArduinoBoardLilyPadUSB)

(Sharp) pictures of the electronics, please. Check if there are good electrical connections. And the bluetooth module is connected to the pins stated in the code. Tx to rx and viceversa