Hi Devs,
I just got my hands on Bluetooth Mate Gold and tried to transmit and receive some data using Arduino Yun and Android app, Bluetooth Terminal, https://play.google.com/store/apps/deta … inal&hl=en.
Here is my Yun code (copied from https://learn.sparkfun.com/tutorials/us … mmand-mode),
/*
Example Bluetooth Serial Passthrough Sketch
by: Jim Lindblom
SparkFun Electronics
date: February 26, 2013
license: Public domain
This example sketch converts an RN-42 bluetooth module to
communicate at 9600 bps (from 115200), and passes any serial
data between Serial Monitor and bluetooth module.
*/
#include <SoftwareSerial.h>
int bluetoothTx = 2; // TX-O pin of bluetooth mate, Arduino D2
int bluetoothRx = 3; // RX-I pin of bluetooth mate, Arduino D3
SoftwareSerial bluetooth(bluetoothTx, bluetoothRx);
void setup()
{
Serial.begin(9600); // Begin the serial monitor at 9600bps
bluetooth.begin(115200); // The Bluetooth Mate defaults to 115200bps
bluetooth.print("$"); // Print three times individually
bluetooth.print("$");
bluetooth.print("$"); // Enter command mode
delay(100); // Short delay, wait for the Mate to send back CMD
bluetooth.println("U,9600,N"); // Temporarily Change the baudrate to 9600, no parity
// 115200 can be too fast at times for NewSoftSerial to relay the data reliably
bluetooth.begin(9600); // Start bluetooth serial at 9600
}
void loop()
{
if(bluetooth.available()) // If the bluetooth sent any characters
{
// Send any characters the bluetooth prints to the serial monitor
Serial.print((char)bluetooth.read());
}
if(Serial.available()) // If stuff was typed in the serial monitor
{
// Send any characters the Serial monitor prints to the bluetooth
bluetooth.print((char)Serial.read());
}
// and loop forever and ever!
}
I debugged the code, below loop from “void loop()” is never entered,
if(bluetooth.available()) // If the bluetooth sent any characters
{
// Send any characters the bluetooth prints to the serial monitor
Serial.print((char)bluetooth.read());
}
Connection between Yun and BT Mate was as shown below,
https://cdn.sparkfun.com/assets/0/c/d/3 … 8b4567.pngI am able to send messages from Arduino IDE Serial Monitor which are received in Bluetooth Terminal app but when I send any messages from the app, serial monitor doesn’t show any message. Connect LED on BT Mate is ON entire time. Also, as explained here, https://learn.sparkfun.com/tutorials/us … mmand-mode, sending “$$$” makes the red LED on BT Mate flash fast but on sending message “E”, monitor doesn’t return any information.
Any help is much appreciated. Thanks in advance.
Jainam