Configure a Lilypad + bluetooth mate

Hi all , not sure if this the right section for this problem …

Im new a this,.

So… im in a school project , the thing is that i bought the Arduino Lilypad and the Bluetooth mate.

now i want to configure it, but i dont know how , here is what i have done to the moment

BT = Bluetooth

–turn on the arduino and BT mate .

–Sync my pc with BT .

–Try to load a script using the arduino program… , this is the point where i fail it gives me that is beeing used so i cant continue to load the program. so ints not a programing problem is when i try conecting or sending info to the arduino… (add info : it conects and uses COM4 , so i configure program to use that COM to … )

Im not sure if this is the way to configure it , hope someone can help me ^^ !

tnx

I haven’t used the Bluetooth mate but my impression from the product page was that this is only used for sending serial data back to the computer. It can’t be used to load programs to the Arduino. You might want to double check that. If not, then using The FTDI is your best bet. Good luck!