Arduino Nano 33 BLE Sense and SparkFun Qwiic OpenLog

Hi,

I posted earlier about this concerning error messages I received when trying to compile any example program for the Qwiic OpenLog using the Arduino Nano 33 BLE Sense. It seems to be at some root level inside both the code for Arduino and Openlog fighting over uint8_t and unsigned char. If someone at SparkFun can get a hold of a Nano 33 BLE Sense, would you please put it on a SparkFun Qwiic shield for Nano and connect the Qwiic OpenLog to it and see if you can reproduce this error. I have about 6 or 7 Qwiic sensors the I am using with this Nano and have successfully compiled and ran the example code for all of them. The Qwiic OpenLog is the only is the only piece of hardware giving me a problem.

Thank you

File an issue here https://github.com/sparkfun/SparkFun_Qw … ary/issues so that the engineers might be able to provide some insight

Hi,

I have posted over on the GitHub forum as requested by you, but no one has addressed this issue on that site either. Can someone at SparkFun please contact the person or persons that can help me with this issue and please help to get it resolved.

Please, Thank you

The engineer(s) assigned to the product get a notification when an issue is created, and it enters there “to do” queue - you should get a notification when a response is added