Good day the forum. In October 2018 I purchased a blackboard Artemis nano. It was a number of months before I could work with it as I was retiring and moving countries (now in Canada).
I have spent the past several weeks trying to get various examples to work with this board. So far the only one that works reliably is the blink example.
I can get no serial window response from the board although it is open in Arduino. The Arduino version is the 1.8.10 and I am working the current (as of Jan. 26, 2020) board definitions.
I can only upload code using the Ambiq secure bootloader and cannot use the Sparkfun Variable Loader.
Help?
Can this board be made to work with the Sparkfun Variable loader?
I am an experienced Arduino coder and have worked with a number of boards including most of the Teensys and the Arduinos.
I have a redboarfd on order but would very much like to get working with the black board.
Best
Mark MacKenzie