Artemis red board

I have 2 red boards and one black board. They all log if i use the USB c connectd to PC. I would like the log the data by just connecting battery ( 3.3v) power on the 2 pin power plug with out using the USB C for power. I like to use the logger as a portable logger, can anybody help me how can i do. If i use the battery connector i see only the red LED on indicating power is on but no blinking LEDs for logger.

Thanks

Hare P

What products are you using? Can you please provide links?

DEV-16832

Are you asking if the OpenLog Artemis (OLA) logs data even when powered by battery? It should if there is an uSD card plugged in the socket.

I want to log data for all sensors when powered by a coin cell or liion battery on the 2 wire power plug. Nothing should be connected to the USB c connector. Portable data looger is what i want

Thanks

Hare

Right, it will log when powered provided that there is something to write to, such as the uSD card. Just ensure that the power supply will be sufficient for powering all the sensors you want connected

power supply is 3.3v battery and the red led light indicator is on. Yes i do have a sd card in there which is properly formatted. But the status led does not flash and there is no data ion the card.

But every thing works well if the USB c connector is plugged.