I’m working on the BR-SC30A, and I have some questions about the AT Command involving the Security.
- I have tried to pair two BR-SC30A together, using AT Command:
“ATPAIR,address”
When it was successfully paired, I tried to unpair them by “ATUPAIR”
, but this’s not working – there was no response “OK”. And I could
not pair one of these two devices to the other BR-SC30A – the
response came up with “PAIR FAILED”.
Also, there was no response for “ATAPAIR” too.
- I saw in the BR-SC30A manual that the Security and Encrytion has a
default as “DISABLE”. I could not find any AT Command to ENABLE it.
I have tried the command: “ATSW24,0,1,0,0” , but not working too.
If anybody knows how to solve these problem or have any suggestions, I’d appreciate.
Thanks