Hi,
I’m new to ARM-USB-OCD with AT91SAM7-P256.
Im trying to run the tutorial LED blinking program but it does not success at 27% with the error below:-
source .gdbinit
target remote localhost:3333
warning: while parsing target memory map (at line 2): Required element is missing
0x00000010 in _vec_dabt ()
monitor soft_reset_halt
requesting target halt and executing a soft reset
monitor armv4_5 core_state arm
core state: ARM
monitor mww 0xffffff60 0x00320100
memory write caused data abort (address: 0xffffff60, size: 0x4, count: 0x1)
monitor mww 0xfffffd44 0xa0008000
monitor mww 0xfffffc20 0xa0000601
monitor wait 100
monitor mww 0xfffffc2c 0x00480a0e
monitor wait 200
monitor mww 0xfffffc30 0x7
monitor wait 100
monitor mww 0xfffffd08 0xa5000401
set remote memory-write-packet-size 1024
set remote memory-write-packet-size fixed
set remote memory-read-packet-size 1024
set remote memory-read-packet-size fixed
monitor arm7_9 force_hw_bkpts enable
force hardware breakpoints enabled
symbol-file main.out
continue
How could I solve this problem??