By powering the Olimex AVR-MT-128 and letting it power the Atmel AVR JTAG
I see the example code start up and display “AVR-MT-128” in the LCD display, and the 2 of the 3 leds is turned on on the AVR JTAG.
After a while the display of the AVR-MT-128 turns off, and there is no action
when pushing the buttons. This is without the AVR Studio running.
It looks like the JTAG resets the MT-128
If I flip the switch on the JTAG to make it self powered, the AVR-MT-128 is started up again, but disappear if I flip it back to taking power from target.
The powersupply I am using is 12V 500mA
If I try to start up AVR Studio wile the MT-128 is alive, I see a sjort blink in the communication led of the JTAG
It is working now, I had to power both the JTAG and the AVR-MT-128 from it’s own powersupply. Is this a standard feature, or is it just my AVR-MT-128 ?