I’m having trouble using the JTAG interface on my Atmega128. I have purchased the Olimex Atmega128 breakout board and the AVR-JTAG adapter. The AVR works fine and I can interact with it via an ICSP connector and PonyProg, however, when I load up AVR Studio and try to connect via JTAG I get nothing. I checked the fuse settings in PonyProg and JTAGEN is checked.
The JTAG connector’s red led doesn’t come on when I power up my circuit. Is there a possibility it is dead?
Help is greatly appreciated…
**EDIT: I checked the power on pins 4 & 7 (VCC) and they read about 2.74v so I do not think it is a power issue.
Someone, anybody? I sent Sparkfun an email monday and a phone call today and I haven’t heard a thing back…
The 7805 regulator needs at least 7V on its input to make +5. Since there is a series diode before the regulator (another 0.7V drop), feed in at least 8V on the “power” connector.
You can also remove the “EPWR” jumper (disconnecting the regulator) and feed 5V in thru pin 1 of the EPWR jumper.