Hello, I’m a newbie to electronics. so please bear with me.
I just got Olimex ATmega128 header board. I looked at the schematic and I’m puzzed where to start
I just want to connect it with power and download simple program using the AVR-USB-JTAG and AVR studio.
I see the power pin labeled power (+). Is this is the one that connects to the source 5v? In the schematic, I see many pins connected to 5v but not sure if I need to connect all the pins labeled 5v to the source power or just the single power 5v pin (labeled +).
Also, in AVR studio do i select JTAGICE or JTAGICE-mkii with the AVR-USB-JTAG?
Thanks a million.