AVR Logic analyzer case and updated source code working!
Hi I found in a forum post the code for a avr logic analyser the avr code works for the arduino so it is a usb logic analyzer.
The pc code is in processing if you use ubuntu linux run processing as root or fallow a tut. in adafruit’s website.
You should load the code into the sketches folder described in the prefrences you find under root. Root is different than normal users folder…
The code can be loaded into a mega 8 or 168 useing usbtiny kit once again I do not have a com port on my laptop.
Using ubuntu once again run the programmer avrdude in root to make the com port work.
Also when running the logic analyzer code make shure your root and your AVR Logic Analyzer is plugged in otherwise you will get a string error because their is not a com port in the string unless your computer has com ports my laptop does not.
This would be a awsome kit and the code realy could use labeling of the channels and port c and arduino pins…
Good cables and case would be great and a time base in the code and graphing allong the time axis…