How to get base location in rover through rtcm data?
As per the Sparkfun library getLatestRTCM1005 API we’ll help to get base location in ECEF format(x,y,z) .Can we convert it into Lat Long format or utm and how accurate it is.
#Ublox_f9p 002B
I’m not sure I understand the question… Accuracy Verification - SparkFun RTK Product Manual and Creating a Permanent Base - SparkFun RTK Product Manual might be helpful (they also use f9p); we also have several extra examples here
clive1
July 18, 2024, 9:30pm
3
/**
******************************************************************************
*
* @file CoordinateConversions.c
* @author The OpenPilot Team, http://www.openpilot.org Copyright (C) 2010.
* @brief General conversions with different coordinate systems.
* - all angles in deg
* - distances in meters
* - altitude above WGS-84 elipsoid
*
* @see The GNU Public License (GPL) Version 3
*
*****************************************************************************/
/*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License as published by
* the Free Software Foundation; either version 3 of the License, or
* (at your option) any later version.
*
* This program is distributed in the hope that it will be useful, but
This file has been truncated. show original
WGS84
a = 6378137.0; // Semi-major earth axis (ellipsoid equatorial radius)
f = 1/298.257223563; // flattening
e = sqrt(f * (2.0 - f)); // eccentricity
thanks @TS-Russell .
Actually I’m not sure about whether rtcm data which rover continuously receive provide base location or not,if yes how to extract that ?
thanks @clive1 .
( getLatestRTCM1005 ) will this API in Sparkfun library giving base point only or other things also?
PaulZC
July 19, 2024, 8:54am
6
Hi Jasvinder (@jasvinder1079 ),
There are RTCM1005 examples in the v3 library:
/*
Get the RTCM 1005 sentence using getLatestRTCM1005
By: Paul Clark
SparkFun Electronics
Date: May 4th, 2023
License: MIT. See license file for more information.
This example shows how to perform a survey-in and then enable RTCM sentences over I2C.
It then demonstrates how to use the new getLatestRTCM1005 function to retrieve the latest RTCM 1005 message.
getLatestRTCM1005 returns immediately - it is not blocking.
It returns:
0 if no data is available
1 if the data is valid but is stale (you have read it before)
2 if the data is valid and fresh
Feel like supporting open source hardware?
Buy a board from SparkFun!
SparkFun GPS-RTK2 - ZED-F9P (GPS-15136) https://www.sparkfun.com/products/15136
SparkFun GPS-RTK-SMA - ZED-F9P (GPS-16481) https://www.sparkfun.com/products/16481
This file has been truncated. show original
/*
Get the RTCM 1005 sentence using a callback
By: Paul Clark
SparkFun Electronics
Date: May 4th, 2023
License: MIT. See license file for more information.
This example shows how to perform a survey-in and then enable RTCM sentences over I2C.
It then demonstrates how to use a callback to retrieve the latest RTCM 1005 message.
Feel like supporting open source hardware?
Buy a board from SparkFun!
SparkFun GPS-RTK2 - ZED-F9P (GPS-15136) https://www.sparkfun.com/products/15136
SparkFun GPS-RTK-SMA - ZED-F9P (GPS-16481) https://www.sparkfun.com/products/16481
Hardware Connections:
Plug a Qwiic cable into the GNSS and a RedBoard
If you don't have a platform with a Qwiic connection use the SparkFun Qwiic Breadboard Jumper (https://www.sparkfun.com/products/14425)
Open the serial monitor at 115200 baud to see the output
*/
This file has been truncated. show original
/*
Use ESP32 WiFi to get RTCM data from Swift Navigation's Skylark caster as a Client, and transmit GGA using a callback
By: SparkFun Electronics / Nathan Seidle & Paul Clark
Date: January 13th, 2022
License: MIT. See license file for more information.
This example shows how to obtain RTCM data from a NTRIP Caster over WiFi and push it over I2C to a ZED-F9x.
It's confusing, but the Arduino is acting as a 'client' to a 'caster'.
In this case we will use Skylark. But you can of course use RTK2Go or Emlid's Caster too. Change secrets.h. as required.
The rover's location will be broadcast to the caster every 10s via GGA setence - automatically using a callback.
This is a proof of concept to show how to connect to a caster via HTTP and show how the corrections control the accuracy.
It's a fun thing to disconnect from the caster and watch the accuracy degrade. Then connect again and watch it recover!
For more information about NTRIP Clients and the differences between Rev1 and Rev2 of the protocol
please see: https://www.use-snip.com/kb/knowledge-base/ntrip-rev1-versus-rev2-formats/
"In broad protocol terms, the NTRIP client must first connect (get an HTTP “OK” reply) and only then
This file has been truncated. show original
The RTCM_1005_data_t struct is defined in u-blox_struct.h:
For a full understanding, you will need to purchase the RTCM Standard:
RTCM 10403.4 defines messages that are used improve the accuracy of location provided by Global Navigation Satellite Systems (GNSS) such as GPS, GLONASS, Galileo, QZSS, BeiDou (BDS), and NavIC. The method used is differential correction which...
Price: USD 340.00
Best wishes,
Paul
Hello @PaulZC ,
This is was through rtcm data to calculate base location points in rover. Is there API or method to get base points from rover directly instead through extracting rtcm frame?
PaulZC
July 20, 2024, 12:42pm
9
Hi Jasvinder,
I do not think that is possible - with u-blox modules.
Best wishes,
Paul