Greetings all.
The subject line says it all; the DRC bot seems to think my silkscreen layers are soldermask when I upload a project. When I upload the gzip file, I specifiy which gerber file is which layer, and the confirmation image I get back always shows the layer mismatch. There’s no silkscreen at all, so those files seem to be ignored entirely. The copper layers are properly rendered.
When I get my PCBs back, everything is fine, but I’m wondering if I’m slowing down the process, by forcing someone to manually adjust the layer assignments. If that’s the case, I hope it’s getting caught before it ruins a panel run.
Is there a naming convention for the layers? I use pcb version 20070208 on Linux; it gives all the layers the suffix “gbr”, but I could easily write a shell script to re-name the layers.
Thanks for any help.