Okay, I’m looking for help with using a relay
to power the Seaflo bilge pump. I’m using
the Beefcake relay board for now.
So, the pump is 12vdc/1.8amps.
I have a 12v, 2A wall wart that I wanted to use for the project.
So, my ignorance is about how to power everything.
Can I use the single 12v 2A power supply for everything?
I was thinking of running a direct line from the 12v source
through the relay, and connecting the pump ground directly to
the source.
And then, also connecting a 7805 to the power supply to power
the micro controller, and ultimately the beefcake brd.
Will this work, or will the 7805 get too hot dissapating the
12vdc?
If heat is a problem, would using a voltage divider before the 7805
solve this? Or would I then have a hot resistor?
A sample circuit diagram would be wonderful, but a few helpful
comments might be enough too.
Thanks.
I want to cycle the pump on for 3 minutes, and then off for 1 minute.
So surges might be an issue too. And I want to be able to change this
interval to, so I want to use a microprocessor to add this feature.