I want to make some “professional” lights with high CRI, because industrial ones are very pricey, so I am going to make my own.
My plan is to make them dim-controllable via bluetooth and arduino with PWM signal.
I use 12 volts 500 mA LED lights (500 mA per half meter). Can I connect three strips in series to each channel of PicoBuck, so I get a load of 36 volts and 500 mA per channel ? I understand that this is the maximum possible load and there is no more backup capacity, which is not good.
For power supply I will use 2 amps 36 volts MeanWell or other good PS.
Can PicoBuck handle it ? Of course LEDs will be attached to the beefy heat sink.