Hello,
I am using the SparkFun bi-directional logic level converter to communicate between a PSoC microcontroller and a 12V water sampler. The sampler will pump water after 12V pulses have been sent to it, and return 12V pulses indicating the sample number and when it is taking the sample. The PSoC microcontroller will only receive and send 3V pulses, but the sampler will only be triggered with a 12V pulse. The logic level converter is being used from the microcontroller to the sampler and from the sampler to the microcontroller. When the wires to the logic level converter are connected and grounded, the HV side of the board is not receiving the pulses from the LV side of the board. When the PSoC microcontroller is in sleep mode and not sending any pulses, the LV side has a low voltage on pins that should not be receiving any voltage and the HV side has pins with a higher voltage that should not have any voltage readings. I have attached an image of the voltages read from a multimeter when the only pins that should have voltage are LV:3.5V and HV:12.4V.
Any insight would be appreciated.