Hi, I’m using your Bi-Directional Logic Level Converter on a breadbord. Now I want to create a PCB and so I’m reproducing the circuit. I see that the component that is used is BSS138. Unfortunately, this component is no more available where I order the components, but it is available BSS138LT3G. Is it good to use instead of BSS138? I need to change 1,8V to 3,3V and 5V to 3,3V for I2C communication.
Thanks for helping.