I’m going to guess that this is constrained by the BlueRadios module-
but
We have a BlueDongle connected to a device that demands no handshake. I can’t find a way to disable the default hardware handshake on the BlueDongle via AT commands, I suppose I could ground-or-high-or -whatever the hardware line, but I haven’t done any serial hardware in years so can’t quite remember if I’m even thinking straigt on that. Is there a way to disable via software?
Also, we need to swap the female jack out for a male jack and, as such, have to swap TX/RX (the gender-changer->null modem->gender changer setup we’re using now is a bit long and cumbersome, heh)