Here’s the issue: The pc gets no data recieved from the device. When i fire up hyperterminal, the status window (under WinXP) shows data sent when I type characters, but recieved stays at zero. I can send AT (with or w/o carrage return) and get no response back.
I’ve tried the other com port that shows up, various hyperterm settings (baud, flow control, etc) and get nothing. I’ve tried sending +++ and $$$ in the first 60 seconds, but all I get is the solid green LED instead. I also have JD1 bridged, and tried it with it unbridged too.
The main issue for all this is I’m using this on a device to connect to a PC wirelessly. In the program that uses that device (moates.net’s Demon), it will not connect fully. I have to change the baud so it works properly.
So is this user error or a faulty device?