Could anyone here help me shed some light on why I can’t get my Bluetooth Mate to work properly with the serial protocol OpenMoco uses?
See link: http://openmoco.org/node/140 I’m new to all this, so I’m not sure what is happening or how best to figure this out.
I have been able to send simple data back and forth from my Arduino Pro using the Arduino IDE’s Serial Monitor window, but when I run the OpenMoco Code on my Arduino Pro and try to send it commands from the SLIM interface over BlueTooth it fails to preform the command or respond at all.
The BlueTooth Mate is showing a green connection LED when I tell SLIM to connect like it did when I tested in IDE Serial Monitor window.
Controlling the OpenMoco Engine via SLIM over a USB connection works just fine, but doing the same thing over a Bluetooth connection fails to respond and times out… I even tried slowing down the Bluetooth Mate to 9600bps to match the USB serial speed and it still didn’t work.
Any Ideas?
This is the OpenMoco code link: http://openmoco.org/node/23
and this is the link for the comand line interface you use to send the serial commands: http://openmoco.org/node/99