Bluetooth Module

Hello,

I have seen the SMD Module - RN-41 (v6.15) which is bluetooth module. Is this module will work like what i expected?.

  1. I want a module which should interface to my microcontroller(say STM32) through UART and it should act as master.

  2. It should paired to only authorized device(means by giving/Setting password).

  3. If the slave bluetooth device access with same password what we set a password for this module, module should callback that, the following device are paired. So that i can unpaired to those device which is not related to my network.

Can any one tell the following features are there in this module.

I am afraid I dont understand your last point completely but it can certainly do the other two things you want it to do.