All PCBs are routed to the given border - not at inch increments.
Example:
If you PCB is 2.15x2.2", your overall cost is 4.73", round up, 5 square inches. BUT your board is actually cut to 2.15" and 2.2".
Each PCB is routed to the obvious edge. You can have a non-square border including simple curves and odd-shapes to fit into enclosures. Please don’t get too creative as Gold Phoenix may revoke this if the complexity of the board orders get out of hand.
Amazingly, Gold Phoenix willallow us to route any contour. Including, L shapes, notches on the corners, circles, Pac-Mac Ghost shapes, etc.
I’ve been reserved about advertising this because I am worried that customers will get a little too creative with their board outlines.
Please, no internal routes, no chinese PCB throwing stars (it would be cool, no?), etc.
Circles are ok. Please do calculate the largest square PCB size as we still have to pack your order onto the panel and circles will inccur a lot of wasted space.
so if i have a board 10 in by 10 in square and I get a 9.5 in square routed out of the middle to make me a nice copper clad frame for only 10 square inches?!? :shock:
I used a rectangular border on the component side silkscreen layer. I had a couple of connectors that hung off so in my email message I included a note saying “please use the rectangular border on the silkscreen – just cut off the connectors that hang over”. That was exactly what I got back. They want enough information so they don’t end of having to guess.
Actually - a border on the silkscreen layer is ideal. We know where the layer is in the CAD program but the guy in china cutting them apart can see the border.
Isn’t this an automated function, using CNC, and thus there doesn’t have to be a visible boarder?
Sparky:
…a border on the silkscreen layer is ideal…
Is this just to help you guys when you panelize (because I haven’t included a border in the silkscreen layer in the boards I’ve ordered) If you would prefer this, I’ll start including it.